Instrument Basic Settings
Configure basic settings of the instrument without navigating to Instrument View or expanding the Settings panel.
For advanced settings, see Instrument Settings.
When the output is on, you cannot change the following settings. To change the settings, turn the output off.
| Output Off/On | Enable (On) or disable (Off) all outputs. |
| Output Coupling | Select output coupling: ACDC – AC superimposed on the DC output AC – AC output DC – DC output |
| Voltage Range | Limit the output voltage range (L or H). |
| Output Mode | Select output mode: 1P – Single phase output 1P3W – Single-phase three-wire output 3P – Three-phase output |